CO2 can be transported in the gaseous phase or in the liquid phase. Liquefaction reduces the volume considerably, making both storage and transport, even over longer distances, more economical. Pipelines would also be much smaller, reducing costs. In addition, CO2 must be pipeline-ready in terms of the contaminants present. Contaminants such as water can cause large-scale corrosion of pipelines and equipment. Less than 50 ppm water is the standard. H2S content in CO2 must also be limited to prevent corrosion at high pressure. CO2 is heavier than air, and any compromise of a transportation pipeline can have devastating consequences for the environment and people.
When transporting CO2 through pipelines and during sequestration, it is important to ensure that the process is carried out at the correct pressure and temperature.