CO2 Transportation, Utilization and Storage

Make your choice


Physics of CO2 

Thermodynamic properties of CO2 for efficient transport and storage
CO2 can be transported in the gaseous phase or in the liquid phase. Liquefaction reduces the volume considerably, making both storage and transport, even over longer distances, more economical. Pipelines would also be much smaller, reducing costs.  In addition, CO2 must be pipeline-ready in terms of the contaminants present. Contaminants such as water can cause large-scale corrosion of pipelines and equipment. Less than 50 ppm water is the standard. H2S content in CO2 must also be limited to prevent corrosion at high pressure. CO2 is heavier than air, and any compromise of a transportation pipeline can have devastating consequences for the environment and people. 

When transporting CO2 through pipelines and during sequestration, it is important to ensure that the process is carried out at the correct pressure and temperature. 

Facts and Figures to remember

  • CO2 in gas state has density of 1.98kg/m3
  • Liquid CO2 occupies 535 times smaller volume compared to gaseous CO2
Beyond the supercritical point, the solid-liquid-gas phases can be in equilibrium.

However, between the critical and supercritical points, the right temperature and pressure can ensure that CO2 remains stable in the liquid phase, which is essential for efficient and safe transport of CO2.

Custody Transfer & Regulations 

Application 3: Custody transfer metering of CO2


The safe transport of CO2 from the capture point to the storage or utilization site is a critical step in the CCS value chain. CO2 is transported in either gaseous or dense phase. A feature of the physical properties of CO2 is that the boundaries that determine the phase change of the fluid are close together. The unique properties of CO2 present several challenges for flow measurement.

  • Accurate and reliable volume measurement with the Promass Coriolis mass flow meter.
  • Expertise in the design, construction and installation of the flow measurement solution
  • Compliance with local and international standards
  • Worldwide references and installed base
Application 3: Custody transfer metering of CO2

Sequestration & Utilization

Carbon storage
CO2 has been used for enhanced oil recovery for almost half a century to increase the recovery factor of oil deposits.

In this case, CO2 is injected in the supercritical phase, where it has the property of behaving like a gas and a liquid at the same time. The density is in the range of liquid CO2, while the viscosity is in the range of gaseous CO2. The dense phase not only helps the oil swell in the reservoir, but also reduces the viscosity of the oil, making it easier to extract.

Another application of CO2 storage is the mineralization of CO2 in rock formations:

Carbfix's innovative technology accelerates the process of rock formation by dissolving CO2 in water and then injecting it into basalt rocks. After injection, it takes 2 years for the rock to carbonize. In this way, the greenhouse gas CO2 is permanently removed from the atmosphere and stored for eternity. 

If you have questions like: 
What is your incentive for deploying CC technology?
Would you like to gain insight into the UK's vision for decarbonizing its hard-to-delete industries? 


Visit the CCSA website to learn more. 

Our offering

FLOW MEASUREMENT

Proline Promass O 500 Coriolis flowmeter

Robust high-pressure flowmeter, as remote version with up to 4 I/Os


Global Energy Transition Masterclass recording now available!

Did you miss our live event? The recording is now available to watch on demand! If you are involved in the global energy transition in your company or simply want to learn which technical solutions are used to achieve the Net-Zero target, this masterclass is for you! 
Language: English


Keynote speakers: 
  • Ruth Herbert, CEO of the Carbon Capture and Storage Association (CCSA), United Kingdom
  • Magnús Þór Arnarson, EPC Project Management at Carbfix, Iceland
  • Martin Voigt, Geochemist at Carbfix, Iceland
  • Nathalie Casas, Head of Technology at Climeworks, Switzerland
  • Khalifa Suhail Barshoud, Section Leader at ADNOC Refining, UAE
  • Florian Kiefer, Senior Scientist and Process Engineer at Empa, Switzerland
  • Marc Allen, Technical Director at engeco, Australia
Ready to watch on demand!

I hereby confirm that I would like to receive regular email updates from Endress+Hauser including promotional material. I can revoke this consent at any time.

By submitting this form I confirm to have read and understood the Privacy Policy*

Copyright © Endress+Hauser Group Services AG      Privacy policy      Legal information      Terms of use      Imprint      Contact
Copyright © Endress+Hauser Group Services AG

Privacy policy      Legal information      Terms of use      Imprint      Contact
Copyright © Endress+Hauser Group Services AG
Privacy policy
Legal information
Terms of use
Imprint
Contact
 
Copyright © Endress+Hauser Group Services AG
Privacy policy
Legal information
Terms of use
Imprint
Contact