This is the most popular method of removing the unavoidable and historic CO2 in our atmosphere.
In this process, tons of air are extracted from the atmosphere. The carbon dioxide is captured on the surface of a highly selective filter material located inside the collectors. After the filter material is filled with carbon dioxide, the collector is closed and the temperature is raised to 80 to 100 °C - this releases the carbon dioxide. Finally, we can collect this high-purity, high-concentration carbon dioxide.
More than 50 countries now practice direct capture of carbon dioxide from the air, and that number continues to grow. The captured CO2 is often used to improve agricultural production in greenhouses.