QUESTION: Is there anything to consider when measuring the temperature in an electrolysis application?
For hydrogen applications, we recommend using austenitic steel thermowells with a higher nickel content.
For high temperature applications, you have to consider H2 diffusion through the steel.
In this case, we would use an adapted thermometer connection head to prevent H2 from "creeping" further into the measuring insert.
QUESTION: What are the most important points to consider when choosing the right flow meter for H2?
QUESTION: Are there material combinations to consider for H2 in flow applications?
We follow ASME standard B31.12, as should any supplier.
QUESTION: What experience do we have in measuring H2 flow rates - can you name some applications?
H2 is traditionally a feedstock for the chemical and petrochemical industries, and we have been supplying the refining, ammonia and petrochemical industries for years.
H2 is used in these applications at low pressure (about 67 bar), for example in amine absorption, a gas treatment process very well known in the natural gas industry to remove CO2 and H2.
QUESTION: Hydrogen is used in refineries for hydrogenation processes such as hydrocracking and hydrotreating. I assume we are working with lower hydrogen pressures there. How different is it in the new applications?
In any case, the H2 gas is used to improve the hydrogen-carbon ratio in the cracked molecules to obtain a wider range of products such as gasoline or kerosene. This application takes place under low pressure conditions.
As the world is looking for cleaner alternatives to reduce CO2 emissions, H2 represents the best alternative to replace fossil fuels in the long term. Therefore, H2 is treated not only as a raw material, but as a main energy source, and we therefore see the demand for larger dimensions for the transportation of H2 and applications with higher pressure, for example, for H2 transport economy.
QUESTION: Is it the same for alkaline electrolyzers and PEM electrolyzers?
In terms of process conditions, the two are completely different, as the process conditions for PEM electrolyzers are more demanding, the pressure requirements are higher (up to 80 barg) and the temperatures reach up to 100 oC. In contrast, the process conditions for alkaline electrolyzers are up to 3 barg higher (there are major differences here), and alkaline electrolyzers have been used in industry for many years.
The efficiency of PEM electrolyzers is also higher than that of alkaline electrolyzers.
QUESTION: Which flowmeter do you recommend for the hydrogen application in electrolyzers?
As mentioned above, we have been supplying our Coriolis meters in the refinery (amine absorption) for many years, and the electrolyzer is also a low pressure application (<100 barg) that matches the performance and design of our Coriolis meters accordingly.
QUESTION: Hydrogen is the smallest molecule. Can it penetrate the diaphragm during pressure measurement?
Our standard pressure transmitters are 316L stainless steel diaphragms with a thickness of e.g. 50 My. Under certain process conditions - typically it depends on pressure and temperature, but also on the media if it is not pure hydrogen - it can diffuse through these membranes. Under these conditions, atomic hydrogen is produced. Diffusion through the membrane causes hydrogen to gradually accumulate in the pressure transfer fluid (filling oil) located behind the membrane. Subsequently, changes in pressure or temperature can cause the saturation limit of hydrogen in the filling oil to be exceeded, resulting in hydrogen bubbles forming in the oil. This can lead to a short-term zero point shift and, in the case of increased diffusion, even to a malfunction. How can this now be avoided: If you coat the membrane with gold, this will completely prevent diffusion of hydrogen into the interior of the membrane.
Follow-up question: What about other wetted parts?
In this case, the issue is not diffusion, but brittleness. A change in brittleness caused by the penetration and intercalation of atomic hydrogen into the metal lattice.
The most important behavior of metals is that susceptibility to hydrogen embrittlement increases with increasing material strength (hardness). Austenitic materials with high nickel content between 10 and 30 percent are a good choice for hydrogen service. SuperDuplexDuplex or other commonly used materialsalloys such as C22C276 or Alloy 400 are not the best choice in this case, but rather the classic 316L material. Tantalum, for example, can become very brittle when operated with high-temperature oxygen or nitrogen or with hydrogen at any temperature.
QUESTION: Do you have a reference for level measurement in liquid hydrogen storage tanks?
Yes, we have used servo technology. We have installed our Servo gauges in two of the first large-scale storage tanks in Japan, one in onshore storage tank and another in LH2 vessel, which have been in operation for more than 1.5 to 2 years.
Follow-up question: Why did the customer choose Servo?
Servo is proven to be the best technology for cryogenic applications and LNG.
Another key issue that was part of the main discussion was the accuracy advantage of servo technology. The accuracy of servo technology at reference conditions is +/- 0.4 mm, for this application using a mathematical calculation with an estimated density of 0.708 g/cm3 hydrogen, the calculated accuracy is +/- 1.9 mm for a larger displacer of 120 mm and +/- 4.3 mm for an 80 mm displacer. For larger tanks, this difference in accuracy thus corresponds to an enormous amount of money.
QUESTION: In our refinery we have problems with controlling the ratio in SMR, is there any recommendation?
Steam methane reforming is a mature production process that uses high temperature steam to produce hydrogen from a methane source, such as natural gas. In steam methane reforming, methane reacts with steam in the presence of a catalyst to produce hydrogen, carbon monoxide, and a relatively small amount of carbon dioxide. Controlling the ratio is critical for efficient operation. This is made possible by an inline Ram Analyzer that measures the composition of methane, CO, H2 and CO2.